In this project, you’ll learn how to use the free software library PINT and CTIMER drivers to detect button presses and generate PWM control signals. These are presented in the context of a development application to drive a powerful, PAPST industrial 4 wire fan unit. The application has 3 speed settings controlled by the E1 buttons which drive the fan’s speed.
If you only have the E1 board, you can still build the software and test the buttons and PWM output signal using an oscilloscope.
E1 development is fully supported using the MCUXpresso IDE from NXP. Detailed steps of how to install the IDE and SDK on your host PC are given in the E1 Getting Started guide which is here.
A new project will be created, and the source files copied into a directory under your workspace.
MCUXpresso Clocks Tool can be used to set the System Clock to the correct frequency for the E1 board. Full details of how to set the system clock on the E1 can be found in this tutorial.
The default project sets the System Clock at 150MHz for use with an external 32MHz crystal source via the Phase-locked Loop (PLL). The E1 board does not have the 32MHz external crystal fitted, so this setting cannot be used.
The clocks view will open showing the clock configuration.
The system clock is now set at 96MHz driven from the 96MHz FRO. The IDE will return to the developer view.
MCUXpresso pins tool can be used to configure the CTIMER mapping to the LEDR pin which generates a PWM output signal. Interrupts can be set on the E1 buttons to detect button presses. The pins tool will generate the source code to include in the build.
Pin mappings for the project:
Name | Function | Board Pin |
red LED | PIO1_4 | LEDR |
ISP button | PIOO_5 | PIOO_5 |
user button | PIO1_9 | PIO1_9 |
wake button | PIO1_18 | WAKE |
The Pin Configuration view will open, displaying the default pin settings.
Pin LEDR on the E1 board is now mapped to CTIMER2.
PIO0_5 button on the E1 board is now mapped to PINT0.
Pins tool will generate the configuration code in pin_mux.h / pin_mux.c.
The IDE will return to the developer view once the source code has been updated.
The project can now be built and tested using the built-in debugger. The PWM output can be checked using an oscilloscope connected to the LEDR output pin and GND on the E1.
/*
* Copyright 2016-2020 NXP
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without modification,
* are permitted provided that the following conditions are met:
*
* o Redistributions of source code must retain the above copyright notice, this list
* of conditions and the following disclaimer.
*
* o Redistributions in binary form must reproduce the above copyright notice, this
* list of conditions and the following disclaimer in the documentation and/or
* other materials provided with the distribution.
*
* o Neither the name of NXP Semiconductor, Inc. nor the names of its
* contributors may be used to endorse or promote products derived from this
* software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND
* ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
* WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE FOR
* ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES;
* LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON
* ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS
* SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
#include <stdio.h>
#include "board.h"
#include "peripherals.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "LPC55S69_cm33_core0.h"
#include "fsl_debug_console.h"
#include "fsl_ctimer.h"
#include <stdbool.h>
#include "fsl_pint.h"
/*******************************************************************************
* Definitions
******************************************************************************/
// PWM
#define CTIMER CTIMER2 /* Timer 2 */
#define CTIMER_MAT_OUT kCTIMER_Match_1 /* Match output 1 */
#define CTIMER_CLK_FREQ CLOCK_GetCTimerClkFreq(2U)
// Fan Speeds - Duty Cycle %
#define OFF 0U
#define LOW 20U
#define HIGH 40U
/*******************************************************************************
* Variables
******************************************************************************/
volatile uint8_t g_state = 0U; // Fan state 0, 1, 2
volatile uint8_t g_pwmDutyCyclePercent = 100U;
volatile uint32_t g_pwmPeriod = 0U;
volatile uint32_t g_pulsePeriod = 0U;
/*******************************************************************************
* Code
******************************************************************************/
status_t CTIMER_GetPwmPeriodValue(uint32_t pwmFreqHz, uint8_t dutyCyclePercent, uint32_t timerClock_Hz)
{
/* Calculate PWM period match value */
g_pwmPeriod = (timerClock_Hz / pwmFreqHz) - 1;
/* Calculate pulse width match value */
if (dutyCyclePercent == 0)
{
g_pulsePeriod = g_pwmPeriod + 1;
}
else
{
g_pulsePeriod = (g_pwmPeriod * (100 - dutyCyclePercent)) / 100;
}
return kStatus_Success;
}
/*!
* @brief Call back for PINT Pin interrupt 0-7.
*/
void pint_intr_callback(pint_pin_int_t pintr, uint32_t pmatch_status)
{
g_state = pintr;
}
/*!
* @brief Set fan speed according to system state triggered by pintr.
*/
void updateFanSpeed(uint8_t state)
{
uint8_t fanSpeed;
switch(state){
case 0: // ISP
fanSpeed = OFF;
break;
case 1: // USER
fanSpeed = LOW;
break;
case 2: // WAKEUP
fanSpeed = HIGH;
}
g_pwmDutyCyclePercent = 100 - fanSpeed; // Invert duty cycle percentage
PRINTF("rnFan speed: %d%%", fanSpeed);
CTIMER_UpdatePwmDutycycle(CTIMER, CTIMER_MAT_OUT, g_pwmDutyCyclePercent);
}
/*
* @brief Application entry point.
*/
int main(void) {
ctimer_config_t config;
uint32_t srcClock_Hz;
uint32_t timerClock;
/* Init board hardware. */
BOARD_InitBootPins();
BOARD_InitBootClocks();
BOARD_InitDebugConsole();
/* Use 12 MHz clock for some of the Ctimers */
CLOCK_AttachClk(kFRO_HF_to_CTIMER2);
/* CTimer0 counter uses the AHB clock, some CTimer1 modules use the Aysnc clock */
srcClock_Hz = CTIMER_CLK_FREQ;
CTIMER_GetDefaultConfig(&config);
timerClock = srcClock_Hz / (config.prescale + 1);
CTIMER_Init(CTIMER, &config);
/* Setup CTIMER match for 1kHz PWM signal with 100% dutycycle */
CTIMER_GetPwmPeriodValue(1000, g_pwmDutyCyclePercent, timerClock);
CTIMER_SetupPwmPeriod(CTIMER, CTIMER_MAT_OUT, g_pwmPeriod, g_pulsePeriod, false);
CTIMER_StartTimer(CTIMER);
PRINTF("CTimer configured to generate a PWM signalrn");
/* Initialize PINT */
PINT_Init(PINT);
/* Setup Pin Interrupt 0 for rising edge */
PINT_PinInterruptConfig(PINT, kPINT_PinInt0, kPINT_PinIntEnableRiseEdge, pint_intr_callback);
/* Enable callbacks for PINT0 by Index */
PINT_EnableCallbackByIndex(PINT, kPINT_PinInt0);
#if (FSL_FEATURE_PINT_NUMBER_OF_CONNECTED_OUTPUTS > 1U)
/* Setup Pin Interrupt 1 for falling edge */
PINT_PinInterruptConfig(PINT, kPINT_PinInt1, kPINT_PinIntEnableFallEdge, pint_intr_callback);
/* Enable callbacks for PINT1 by Index */
PINT_EnableCallbackByIndex(PINT, kPINT_PinInt1);
#endif
#if (FSL_FEATURE_PINT_NUMBER_OF_CONNECTED_OUTPUTS > 2U)
/* Setup Pin Interrupt 2 for falling edge */
PINT_PinInterruptConfig(PINT, kPINT_PinInt2, kPINT_PinIntEnableFallEdge, pint_intr_callback);
/* Enable callbacks for PINT2 by Index */
PINT_EnableCallbackByIndex(PINT, kPINT_PinInt2);
#endif
PRINTF("rnPINT Pin Interrupt events are configuredrn");
PRINTF("rnPress ISP (OFF), USER (LOW), WAKE (HIGH) to set fan speedrn");
while (1)
{
__WFI();
updateFanSpeed(g_state); // Update fan speed
}
}
The project will build without errors, shown in the Console pane.
The IDE will discover the LPC11U3x_CMSIS_DAP debug probe.
The Printf statements will appear in the Console pane when buttons ISP, USER & WAKE are pressed.
The PWM signal can be seen on the oscilloscope – the signal on the LEDR pin has the duty cycle inverted to control the brightness of the LED correctly. High being OFF and Low being ON.
A 30V / 5A DC bench power supply connects to the +24V and GND terminals for the fan. The linear voltage regulator has its input connected to the +24V rail of the fan circuit. A general-purpose diode provides reverse polarity protection and 1uF bypass capacitors provide filtering. The regulators 5V output connects to the 5V rail which powers the E1 via its 5V pin. The E1 GND pin is connected to GND. The E1 has an onboard LDO regulator (Maximum input 6V) that outputs 3.3V to VDD.
E1 pins have a maximum voltage rating of 3.3V – do not connect any higher voltages as this may damage the board.
An N-Channel MOSFET inverts the PWM signal from the LEDR pin. It also isolates the pin from any higher voltages. The LEDR output is connected to the Gate of the MOSFET via a 1k resistor, while a 10k resistor is connected between 5V and Drain. The MOSFET source is connected directly to GND. The Papst fan used in the example requires a 1 – 5kHz PWM signal on its open collector input. This is connected between the Drain of the MOSFET and the 10k resistor. When the Gate of the MOSFET is driven HIGH, the PWM output is driven LOW and vice versa.
The controller has 3 speeds, OFF (ISP), LOW (USER) and HIGH (WAKE) set by pressing one of the E1 buttons. Interrupts connected to the buttons cause the system status to update which changes the PWM duty cycle which controls the fan. Once a button has been pressed, the system then waits for the next interrupt.
Check the pinout of your MOSFET as it may be different from the one shown in the circuit diagram.
This guide has shown you how to start a new E1 project using MCUXpresso IDE and to use the PINT and CTIMER drivers included in the SDK. The example is used to create an application that drives a PWM controlled fan unit using button interrupts on the E1 board.
We showed how the Clocks and Pins tools built into MCUXpresso IDE can be used to generate pin configuration code to ease development of complex applications and minimise coding. This allows the developer to concentrate on the application logic.
The SDK provides several demo apps that show how to use many other free peripheral drivers that can be used in your own code or as a starting point for applications.
From a quick tap to smashing that love button and show how much you enjoyed this project.