Raspberry Pi 3

Our Raspberry Pi 3 range showcases the third edition of the Raspberry Pi microcomputer family. The original Raspberry Pi 3 Model B was first released in 2016, with the Model B+ and A+ following in 2018. The Raspberry Pi 3 board is a gamechanger in that it is the first to open up Wi-Fi and Bluetooth connectivity abilities, making it easier to communicate with other supported devices. The Model B offers other upgrades over its predecessors, including an impressive running speed of 1.2GHz. For something even more powerful, look to the Raspberry Pi 3 B+. It comes with a 1.4GHz processor and other great performance improvements. The Raspberry Pi 3 Model A+ meanwhile is a lower-cost, slimmer option with the same computing power and functionality, but one USB port rather than four. Whatever your Raspberry Pi 3 model of choice, you will find the possibilities are endless with this fast and versatile device. View more View less

10 items

Privacy

Our website uses cookies and similar technologies to provide you with a better service while searching or placing an order, for analytical purposes and to personalise our advertising. You can change your cookie settings by reading our cookie policy. Otherwise, we’ll assume you’re OK with our use of cookies.

Location

Please select an option to see content specific to your location and shop online.

Browse the US site