Raspberry Pi 2

The Raspberry Pi 2 board is the second generation in the iconic Raspberry Pi microcomputer series. First released in February 2015, this successor offers more power and memory space for even greater project possibilities. You can choose from the two versions available below. The Raspberry Pi 2 Model B is a small, smart device that boasts an increased processor speed of 900MHz, 1GB of RAM and four USB ports. You will find that the Broadcom System on Chip and CPU are also upgraded from the Raspberry Pi 1 Model B+. A further step up comes in the shape of the Raspberry Pi 2B V1.2 device which was released slightly later. The Broadcom System on Chip and processor are again updated to provide noticeable performance improvements. Whichever Raspberry Pi 2 computer you opt for, you can simply plug in your TV or monitor using the HDMI port, add a keyboard, mouse and power supply, and get creating. View more View less

2 items

Privacy

Our website uses cookies and similar technologies to provide you with a better service while searching or placing an order, for analytical purposes and to personalise our advertising. You can change your cookie settings by reading our cookie policy. Otherwise, we’ll assume you’re OK with our use of cookies.

Location

Please select an option to see content specific to your location and shop online.

Browse the US site