Ever written your name with a sparkler? Seen long-exposure photos of cities at night where the car tail-lights leave long streaks of light across the scene? Using the same principles you can make a rainbow painting magic wand out of addressable LEDs and a Gemma microcontroller.
To programme the Gemma, we’ll be using the Arduino IDE.
The next step is to connect our pixels to the Gemma, being careful not to touch the crocodile clips together. You can ignore the cardboard on the photo.
A common mistake people make is to connect from the wrong end of the strip. Check that the arrows on it point away from where you have just connected the crocodile clips.
When you installed the libraries for the Gemma on the Arduino IDE, several sample programs were installed too. You can use one of these to test your strip.
You will need to change two numbers in the programme.
Change LED_PIN 6 to LED_PIN 1. This defines which pin on the Gemma will connect to the LEDs.
Change LED_COUNT 60 to LED_COUNT 7. This defines how many LEDs we’re using.
Once the changes have been made, save it as a copy renaming it to whatever you want.
Connect the Gemma to your computer using the micro USB cable. Make sure the Gemma’s switched on.
Load the code to the Gemma by pressing the reset button and then pressing the upload button in the Arduino IDE, this is the right-pointing arrow.
If you get an error while uploading, check that you have the correct board selected, the correct programmer for your particular board, and that the board is connected via USB to your computer.
You should still have the program that you loaded onto the device and tested earlier. If you turn on the Gemma (also making sure that the battery pack is turned on) everything should light up as before. If it doesn’t:
If it works, you can go ahead with trying out your camera settings using the sample program.
With the wand we made, there are 7 pixels, and they are lit from the bottom up, so the pixel nearest the Gemma is pixel 0, the next one pixel 1, and so on until the one at the top of the stick, which is pixel 6. If we want a rainbow from the top-down, pixel 6 needs to be red, pixel 5 needs to be orange, pixel 4 yellow, and so on.
// Modified from:
// NeoPixel Ring simple sketch (c) 2013 Shae Erisson
// Released under the GPLv3 license to match the rest of the
// Adafruit NeoPixel library
#include <Adafruit_NeoPixel.h>
#ifdef __AVR__
#include <avr/power.h> // Required for 16 MHz Adafruit Trinket
#endif
// Which pin on the Arduino is connected to the NeoPixels?
#define PIN 1 // On Trinket or Gemma, suggest setting this to 1
// How many NeoPixels are attached to the Arduino?
#define NUMPIXELS 7 // Set to rainbow painter stick
// When setting up the NeoPixel library, we tell it how many pixels,
// and which pin to use to send signals. Note that for older NeoPixel
// strips you might need to change the third parameter -- see the
// strandtest example for more information on possible values.
Adafruit_NeoPixel pixels(NUMPIXELS, PIN, NEO_GRB + NEO_KHZ800);
void setup() {
// These lines are specifically to support the Adafruit Trinket 5V 16 MHz.
// Any other board, you can remove this part (but no harm leaving it):
#if defined(__AVR_ATtiny85__) && (F_CPU == 16000000)
clock_prescale_set(clock_div_1);
#endif
// END of Trinket-specific code.
pixels.begin(); // INITIALIZE NeoPixel strip object (REQUIRED)
}
void loop() {
pixels.clear(); // Set all pixel colors to 'off'
// The first NeoPixel in a strand is #0, second is 1, all the way up
// to the count of pixels minus one.
{ // For each pixel...
// pixels.Color() takes RGB values, from 0,0,0 up to 255,255,255
// The one closest to the Gemma is pixel 0
// The one furthest away is pixel 6
// These are set up as a rainbow, but you can choose your own colours.
pixels.setPixelColor(6, pixels.Color(100, 0, 0)); // red
pixels.setPixelColor(5, pixels.Color(130, 40, 20)); // orange
pixels.setPixelColor(4, pixels.Color(100, 100, 0)); // yellow
pixels.setPixelColor(3, pixels.Color(0, 100, 0)); // green
pixels.setPixelColor(2, pixels.Color(0, 0, 100)); // blue
pixels.setPixelColor(1, pixels.Color(100, 0, 230)); // indigo
pixels.setPixelColor(0, pixels.Color(200, 0, 230)); // violet
pixels.show(); // Send the updated pixel colors to the hardware.
}
}
On our phone, we used “pro” mode on the camera to capture these images. Pro mode lets you choose how long the shutter is open for, and the “speed” of the film. We used the following settings:
ISO = 64
Shutter = 10 seconds F1.5
To get good low light photos you will have to fiddle with the settings until you get them just right. These were taken in a field away from any street lighting, but for you, you may have to increase the ISO or decrease the time the shutter is open for.
If you have an iPhone, you will need a separate app, as the settings on the camera aren’t as accessible. Recommended apps are SlowShutter Cam, and Moment, but other apps are available.
You will also need to put your camera somewhere steady – if you have a professional tripod, great, but if not, propping it up on a garden chair also works!
Camera Settings: ISO 64, 10 second exposure
You may want to alter the program to be the colours that you prefer, to a single pixel, or to various patterns. In the examples in the Adafruit Neopixel library, you will find a variety of programs to experiment with. You could add a mode button to your wand, by connecting it to pin D2 and ground, and use the example titled buttoncycler to switch between patterns.
From a quick tap to smashing that love button and show how much you enjoyed this project.