This is a very simple project, ideal for kids as it uses Scratch, a visual programming environment which is great to start learning about programming. It will see you through some basics of using a Raspberry Pi, programming and circuit making.
You should start the project with an already set-up Raspberry Pi running the latest noobs. You can learn how to do that here.

- Connect a jumper wire to the positive (longer) leg of the LED and to any leg of the 3.3K Ohm resistor
- Connect another jumper wire to the other leg of the 3.3K Ohm resistor
- Connect a jumper wire to the negative (shorter) leg of the LED
It doesn’t matter which colour jumper wires you use, but for clarity, it’s a good idea to use black for negative and red for positive polarities.
Ensure that the resistor is connected to the positive leg of the LED

- Connect mouse, keyboard and monitor to the Raspberry Pi and power it up. You can learn how to do it here
- Connect the jumper wire attached to the resistor to the 3V3 pin (top left) on the Raspberry Pi
- Connect the other jumper wire attached to the resistor to the GND pin (3rd right) on the Raspberry Pi
Your LED should now be on.
This was a quick test to ensure that everything works fine.

- Disconnect the jumper wire attached to the resistor from the 3V3 pin
- Connect the jumper wire attached to the resistor to pin GP25 (11 on the right column)

- Navigate to the Raspberry icon on the top left of your Raspberry Pi’s desktop and open “Scratch 2” from the “Programming“ menu

- Ignore the cat
- Click on “More Blocks”
- Click on “Add an Extension”

- Select “Pi GPIO” and click “Ok”

- From the “Events” menu in Scratch 2, drag “when clicked” into the right-hand panel

- Drag “repeat” from the “Control” menu and attach it to “when clicked”

- Drag “set gpio” from the “More Blocks” menu into “repeat”. Select “25” from the “set gpio” dropdown

- Drag “wait secs” from the “Control” menu and place it under “set gpio”
- Drag another instance of “set gpio” into position and set it to GPIO “25” and “output low”
- Drag another instance of “wait 1 secs”
You’re all set!

- To see your programme in action , click on the green flag on the top right of the Scratch 2 preview window
Your LED should now be flashing on and off every second.
You can experiment with different timings by changing the “wait” timings.