PRESS RELEASE
New E1 board, featuring NXP’s LPC55S69 Microcontroller, offers a high-performance, secure low-cost entry to the IoT
London, UK, Date – OKdo, part of the Electrocomponents Group, today introduced its first own-branded single board computer (SBC), the E1. This represents the start of the next phase in the company’s evolution towards providing an accessible range of software, hardware, services and solutions, and is exclusively available from OKdo.
With its focus on single board computing in the IoT, OKdo is uniquely qualified to bring the E1 to market. Its small form factor provides a host of features to enable users, from makers to industrialists, to develop connected solutions that are robust and secure.
The board, which was developed in collaboration with NXP® Semiconductors, is supported by NXP’s comprehensive software development ecosystem. This includes the full-featured MCUXpresso integrated development environment (IDE), support for other IDEs, as well as a range of middleware and open-source operating systems.
While the board’s host of integrated features can meet the needs of most applications, OKdo has developed the E1 to work well with other open source projects, such as Arduino and Digilent Pmod. A passive companion PCB allows developers to add other functions from the wide range of Arduino-compatible shields, which are also available to purchase from OKdo.
NXP is happy to be involved with this project and we are delighted to collaborate with OKdo on the E1,” said Justin Mortimer, MCU Product Marketing Manager at NXP. “This board demonstrates OKdo’s commitment to bringing advanced technologies at a compelling price point and form factor to a wider audience.”
In addition to forming the basis for secure IoT endpoints, the E1 is a great platform for evaluating NXP’s LPC55S69 microcontroller, a highly capable yet low-power MCU based on the Arm® Cortex®-M33 32-bit processing core, running up to 150MHz. Additionally, the MCU integrates a number of advanced features that are becoming essential in any IoT application, including: a cryptographic co-processor; a DSP hardware accelerator; a security module for the real-time encryption/decryption of information (data and code) stored on the on-chip Flash memory; on-chip ROM; support for secure boot; and a range of digital and analogue peripherals. The MCU is also Arm TrustZone®-M enabled and includes an AES-256 encryption/decryption engine, a physical unclonable function (PUF) for key generation and a true random number generator (TRNG).
“OKdo is all about providing SBC and IoT solutions that can change the world,” commented Richard Curtin, Global SVP Technology at OKdo. “Since our launch in 2019, OKdo has quickly grown into a leading supplier of IoT solutions. The E1 is the first step towards extending that reach, to become a manufacturer of SBCs that can further empower makers and professional engineers to realise their goals even faster. The E1 demonstrates that we are lowering the barriers to entry for more people who want to be part of this technological revolution.”
The E1 single board computer costs £13.42 and is available here
About OKdo
OKdo is a global technology company from Electrocomponents (LSE:ECM) set to disrupt single board computer (SBC) and IoT segments. Offering a unique combination of hardware, software, development support, manufacturing services and community projects, it is the world’s first business uniquely focused on meeting the rapidly evolving needs of SBC and IoT customers, from makers and entrepreneurs to industrial designers, educators and resellers. For more information: www.OKdo.com