OKdo & OStream Unveil New Partnership at CES 2023 for Scalable, Edge AI Media Processing

Edge Supercomputer Delegates AI, Video & CPU Operations to Hardware Accelerated Components Across a Cluster of SBCs.

London, UK, 7th January 2023 – OKdo, the innovative Single Board Computer and Internet of Things arm of RS Group plc, announced a global partnership with OStream, the leading innovator for Edge AI media processing infrastructure.

The technology partnership will allow integrators to enrich video and audio streams with the context to take real-time action at the edge while delivering image search engine features in their applications. The modular, clustered approach allows for right-sized scaling from pilot (3 TOPs) to production (800 TOPs) all in one hardware unit. PipeRunner modules are based on NVIDIA ORIN and Rockchip NPUs, computer vision specific CPUs and video encoders/decoders. The solution is deployed on the Edge and pulls media streams from already deployed cameras in the environment.

OKdo has licensed OStream’s PipeRunner technology that automatically delegates Edge AI operations to the most optimised hardware component available across the cluster. AI operations run on NPUs, video on VPUs and computer vision tasks on CPUs. Historically, integrators are forced to choose between vertically scaled servers that offer static amounts of AI and CPU but no dedicated video processing. PipeRunner’s horizontal design lets customers stack up NPU, CPU and VPU modules to previously unachievable scale.

The partnership will establish a secondary track to OKdo’s SBC roadmap. OKdo’s primary track of SBCs focuses on CPU bound applications with their Rock boards and modules. OKdo PipeRunner will offer a separate track of boards that feature the trifecta of hardware acceleration from NPU, VPU and CPU coupled with the software to make it run smoothly at any level of expertise. The cluster software will come as standard on OKdo boards in this track offering a powerful layer that allows developers to deliver value faster. PipeRunner CEO, Kerry Shih, says “PipeRunner allows integrators to build horizontal, media processing solutions that scale up to 800 TOPs per device by clustering SBCs and surrounding it with video hardware acceleration and high-speed backplane.”

OKdo CTO, Richard Curtin, adds “While the demand for AI applications at the Edge is at an all-time high, the SBC boards and software stacks offered today create too much work for integrators. We want to enable highly scalable AI applications without developers losing sleep over whether it will perform.” OKdo touts that the horizontal model of building AI supercomputers out of SBCs is far more cost effective than the more limited and expensive vertical model.

OKdo promotes PipeRunner as being useful for makers and industrial integrators alike. It has been deployed with customers including a Fortune 100 company, several international integrators and bundled by a leading camera company. PipeRunner is designed to stream video and audio from cameras, execute AI models against the media and enrich the resulting metadata into the Object MP4 format. The extended format allows customers to take real-time action at the Edge and build a data lake of searchable media.

About OKdo

OKdo is a global technology company, an operating brand of RS Group plc (LSE:RS1), which is disrupting single board computer (SBC) and IoT segments. Offering a unique combination of hardware, software, development support, manufacturing services and community projects, it is the world’s first business uniquely focused on meeting the rapidly evolving needs of SBC and IoT customers, from makers and entrepreneurs to industrial designers, educators and resellers.

For more information contact: katie.chubb@okdo.com

www.okdo.com | Twitter | YouTube | LinkedIn | Facebook | Instagram

About OStream
OStream is the leading innovator for enriching media streams with the context to trigger real-time action and offer intuitive search at scale. Its software and reference designs are available for licensing by device makers worldwide. The founders are 20 year veterans in IoT, video, streaming media and AI. The company is primarily located in Los Angeles and is privately funded.

For more information contact: bill@ostream.com

Copyright ©2022 OStream Inc. All rights reserved. OStream and Percept are trademarks of OStream Inc. Other trademarks are the property of their respective owners.

Privacy

Il nostro sito web utilizza cookie e altre tecnologie simili per fornirti un servizio migliore quando effettui una ricerca o fai un ordine, per finalità analitiche e per personalizzare la nostra pubblicità. Puoi modificare le tue impostazioni per i cookie leggendo la nostra politica sui cookie. In caso contrario, supporremo che accetti il nostro utilizzo dei cookie.

Location

Please select an option to see content specific to your location and shop online.

Browse the US site