This project shows you how to convert a Nintendo console gamepad into a USB keyboard controller. The gamepad will be recognised as a keyboard by your computer. Each button will output a different letter. You can then map this to the controls of any game. There are many variants of the SNES gamepad so the images here might not exactly match your controller physically. You should be able to use these instructions as a guide for any SNES gamepad.
Using the same technique as above, solder the following wires to the buttons. Ensure that you solder to the live connector on each button, not the one connected to ground.
Using the same process as before, solder the following:
Now we’ll solder all the wires to the Teensy, starting with the first ribbon, to do this you’ll need a vise or helping hands to hold the Teensy while you do the soldering.
Next we’ll solder the other ribbon cable.
To programme the Teensy you’ll need Arduino IDE and Teensyduino installed on your computer.
Upload the following code.
#define REPEATRATE 100 // milliseconds
const int pinBtnUp = 0;
const int pinBtnRight = 1;
const int pinBtnDown = 2;
const int pinBtnLeft = 3;
const int pinBtnSelect = 4;
const int pinBtnStart = 5;
const int pinBtnB = 7;
const int pinBtnA = 8;
const int pinBtnY = 10;
const int pinBtnX = 9;
const int pinBtnTrigLeft = 6;
const int pinBtnTrigRight = 23;
const int pinLEDOutput = 11;
//Variables for the states of the SNES buttons
byte buttons[] = { pinBtnUp, pinBtnRight, pinBtnDown, pinBtnLeft, pinBtnSelect, pinBtnStart,
pinBtnB, pinBtnA, pinBtnY, pinBtnX, pinBtnTrigLeft, pinBtnTrigRight
};
unsigned int keys[] = {KEY_U, KEY_R, KEY_D, KEY_L, KEY_ENTER, KEY_TAB, KEY_B, KEY_A, KEY_Y, KEY_X, KEY_P, KEY_Q};
#define NUMBUTTONS sizeof(buttons)
void myset_key1(uint8_t c)
{
Keyboard.set_key1(c);
}
void myset_key2(uint8_t c)
{
Keyboard.set_key2(c);
}
void myset_key3(uint8_t c)
{
Keyboard.set_key3(c);
}
void myset_key4(uint8_t c)
{
Keyboard.set_key4(c);
}
void myset_key5(uint8_t c)
{
Keyboard.set_key5(c);
}
void myset_key6(uint8_t c)
{
Keyboard.set_key6(c);
}
typedef void KeyFunction_t(uint8_t c);
KeyFunction_t* buttonActive[NUMBUTTONS];
KeyFunction_t* keyList[] = {myset_key6, myset_key5, myset_key4, myset_key3, myset_key2, myset_key1};
int keySlot = sizeof(keyList) / sizeof(KeyFunction_t*);
void setup()
{
//Setup the pin modes.
pinMode( pinLEDOutput, OUTPUT );
//Special for the Teensy is the INPUT_PULLUP
//It enables a pullup resitor on the pin.
for (byte i=0; i< NUMBUTTONS; i++) {
pinMode(buttons[i], INPUT_PULLUP);
}
//Uncomment this line to debug the acceleromter values:
// Serial.begin();
for (unsigned int i=0; i < NUMBUTTONS; i++) {
buttonActive[i] = 0;
}
}
void loop()
{
// //debugging the start button...
digitalWrite ( pinLEDOutput, digitalRead(pinBtnStart));
//Progess the SNES controller buttons to send keystrokes.
fcnProcessButtons();
}
//Function to process the buttons from the SNES controller
void fcnProcessButtons()
{
bool keysPressed = false;
bool keysReleased = false;
// run through all the buttons
for (byte i = 0; i < NUMBUTTONS; i++) {
// are any of them pressed?
if (! digitalRead(buttons[i]))
{ //this button is pressed
keysPressed = true;
if (!buttonActive[i]) //was it pressed before?
activateButton(i); //no - activate the keypress
}
else
{ //this button is not pressed
if (buttonActive[i]) { //was it pressed before?
releaseButton(i); //yes - release the keypress
keysReleased = true;
}
}
}
if (keysPressed || keysReleased)
Keyboard.send_now(); //update all the keypresses
}
void activateButton(byte index)
{
if (keySlot) //any key slots left?
{
keySlot--; //Push the keySlot stack
buttonActive[index] = keyList[keySlot]; //Associate the keySlot function pointer with the button
(*keyList[keySlot])(keys[index]); //Call the key slot function to set the key value
}
}
void releaseButton(byte index)
{
keyList[keySlot] = buttonActive[index]; //retrieve the keySlot function pointer
buttonActive[index] = 0; //mark the button as no longer pressed
(*keyList[keySlot])(0); //release the key slot
keySlot++; //pop the keySlot stack
}
Now you can test it.
Open any text editor and press the buttons. You don’t need to assemble the controller, just place the rubber pads over each of the contacts at a time and press. You should be getting:
If all is well we can now reassemble the controller!
There are several variants of the SNES controller, so the exact way in which you’ll do this will be slightly different for each controller. This is the trickiest part of the project and might take a bit of fiddling.
You’re ready to play!
From a quick tap to smashing that love button and show how much you enjoyed this project.