You can easily turn a Raspberry Pi into a webcam for your PC. Whether your laptop’s camera is broken or you need to place the camera looking away from you, this simple solution has you covered. You’ll configure your Pi to make its camera stream available to any computer on your network.
You can now test that the camera is working.
raspistill -o testimage.jpg
This will momentarily bring up a window displaying the camera’s view and after a few seconds, it will take a photo. You can find the photo in Home> Pi> testimage.jpg.
sudo apt-get install cmake libjpeg8-dev -y
sudo apt-get install gcc g++ -y
Now you’ll install the program that takes the camera’s input and shares it on the network.
git clone https://github.com/jacksonliam/mjpg-streamer
cd mjpg-streamer/mjpg-streamer-experimental && make && sudo make install
Mjpeg streamer should now be installed and ready to run.
Start Mjpeg streamer by entering the following:
mjpg_streamer -i input_raspicam.so -o output_http.so
You can test the stream on your PC or on your Pi by opening a browser and going to: http://[raspberrypihostname]:8080?action=stream
The default hostname for the Pi if you haven’t changed it is http://raspberrypi:8080/?action=stream.
Once all this is working, you can tweak the camera’s settings to optimise its performance for your network setup. You can see below the syntax to specify the camera’s settings. You can use whatever works for you but we found 1280×720 at 12 frames per second to be good for our purposes. If your camera feed is stuttering, you can try lower resolution settings like 640×360.
mjpg_streamer -i "input_raspicam.so -x 1280 -y 720 -fps 12" -o output_http.so
Having to start the camera using Terminal is not very convenient. It’s a good idea to set it up so that the camera comes on whenever the Pi starts up.
[Unit]
Description=IP camera streaming service
After=network.target
[Service]
ExecStart=/bin/sh -c 'mjpg_streamer -i "input_raspicam.so -x 1280 -y 720 -fps 12" -o output_http.so'
Restart=always
RestartSec=30
[Install]
WantedBy=multi-user.target
sudo cp mjpg_streamer.service /etc/systemd/system/
sudo systemctl daemon-reload
sudo systemctl start mjpg_streamer.service
sudo systemctl enable mjpg_streamer.service
Now, you’ll need to connect the camera stream to a recognisable webcam to your Windows 10 system.
You should now have an available camera stream to use with your choice of video conferencing app.
Your camera will appear under the name MJPEG Camera. Below you can see this in Google Meet.
From a quick tap to smashing that love button and show how much you enjoyed this project.